Advice to have quickly a K60 with Ethernet Udp/Tcp and Flash driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Advice to have quickly a K60 with Ethernet Udp/Tcp and Flash driver

Jump to solution
620 Views
arnogir
Senior Contributor II

Hello,

We need to develop a bootloader for the K60 via the Ethernet (with BootP protocol).

Currently, I'm using the USB bootloader provided by Freescale.

Then, Are they a fast option to dispose (without need MQX) an application with the layer Ethernet to receive and send UDP/TCP frame, and then a Nandflash driver?

I think there are KDSK, with MCUexpresso? Or other? Are they some exempled? (I already use the MQX Ethernet stack with KDS, but not flash driver).

Thank

0 Kudos
1 Solution
446 Views
miduo
NXP Employee
NXP Employee

Hello,

Maybe you would like to have a look at  FNET Embedded TCP/IP Stack , which provides Ethernet bootloader for K6x chip.

And we also provide an application note for your reference:

https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN4367.pdf 

View solution in original post

0 Kudos
2 Replies
447 Views
miduo
NXP Employee
NXP Employee

Hello,

Maybe you would like to have a look at  FNET Embedded TCP/IP Stack , which provides Ethernet bootloader for K6x chip.

And we also provide an application note for your reference:

https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN4367.pdf 

0 Kudos