The problem has been resolved,to upgrade "win_hc08sprg.exe" version to 10.0.18.0.
However,I got another issue done the AN2295 procedure(User code on 0x00004400).
Can't boot up after AC power.I founded the reset pin always high and low.What happened?
Thanks!
B&R.
AN2295_LinkerFile.icf
>>>>
/*-Memory Regions-*/
define symbol __ICFEDIT_region_ROM_start__ = 0x00000000;
define symbol __ICFEDIT_region_ROM_end__ = 0x00003FFF; // 0x000004FF for 8K Flash devices
define symbol __ICFEDIT_region_RAM_start__ = 0x1fff0000;
define symbol __ICFEDIT_region_RAM_end__ = 0x1fffffff;
define symbol __ICFEDIT_region_RAM1_start__ = 0x20000000;
define symbol __ICFEDIT_region_RAM1_end__ = 0x2000ffff;
define symbol IntVectTable_start__ = 0x00000000;
define symbol IntVectTable_end__ = 0x0000003f;
define symbol FlashConfig_start__ = 0x00000400;
define symbol FlashConfig_end__ = 0x0000040f;
<<<<
define exported symbol __BOOT_STACK_ADDRESS = __ICFEDIT_region_RAM1_end__ - 7; //>>>>>>>> ?????? Is correct?
bootloader.c
>>>>
<<<<
Ahter Running......
>>>>
<<<<
Can't boot up after AC power. Is the entry point uncorrected?