Queries related with KDS and MQXLite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Queries related with KDS and MQXLite

462 次查看
anilnadargi
Contributor II

I have installed KDS version 3.0.0 on windows 7 along with Processor Expert .

 

My Queries are as below .

1. I have KDS version supported MQXLite and does its requires KSDK for MQXLite support ?

 

2. Any example / tutorial project which shows Task using MQXLite and Processor Expert components.

     E.g. : Task using lwevent (MQLite ) and UART ( PE Component )

 

3. What all we require to start MQXLite and PE based project on KDS IDE.

 

Thanks .

标签 (1)
0 项奖励
回复
1 回复

365 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Anil,

1.It doesn't need KSDK .

2. The attachment is a MQXLITE training material , the  honds on is about CodeWarrior  demo , while it is the same on KDS , you can refer to .

And about the UART or ADC component usage, you can refer to the "Typical Usage" of Help on component :

pastedImage_0.png

3.  You only need the KDS , and the "Help on component" on PE is useful when you development  your project use the PE.

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复