MKL17UART does not work at low temperatures

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MKL17UART does not work at low temperatures

1,374件の閲覧回数
gavinyork
Contributor I

MKL17 uart dont`t work at low temp  and when at room temperature to work properly. Why?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,298件の閲覧回数
scottm
Senior Contributor II

If you're running from the internal clock reference, check the frequency drift vs. temperature curve in the datasheet.  Looks like it varies by maybe 0.5% over 20 degrees C, which could be enough to take your baud rate out of spec.

The one time I've gotten a crystal-referenced MCU enough out of spec to be a problem, I had it at about -190 C, just above the liquid level in a dewar of liquid nitrogen.

On the other hand, the first time I used Processor Expert for clock setup I accidentally selected the internal reference instead of external.  My first prototype worked OK but without trimming it was hit or miss on the others.

Scott

0 件の賞賛
返信

1,298件の閲覧回数
bobpaddock
Senior Contributor IV

What exactly is 'Low'?

What is the clock source as that is the most temperature dependent component?

0 件の賞賛
返信