I am attempting to share the TX Pin of a uart of a 120mhz K70.
I have an AsynchroSerial component setup and have the pin shared.
When I generate PE code with the ConnectPin method set to be generated, I get a generator failure error.
Description Resource Path Location Type
Generator: FAILURE: at line 228: Error in including "Drivers\Common\SynchroMasterConnectPin.inc" from directory C:\Freescale\KDS_3.0.0\eclipse\ProcessorExpert\Repositories\Kinetis_Repository (file: Drivers\Kinetis\AsynchroSerial.drv) Series3MQXLiteKDS DMXSerial Processor Expert Problem
This worked fine in CW 10.6
It seems weird that the ASychro component is looking for the SynchroMasterConnectPin file
Any ideas on how to fix this. It also seems to happen on a K10 project.
Tim
已解决! 转到解答。
Hello Tim,
The hot fix is prepared and verified in the KDS 3.0.0 - PEx for Kinetis 3.0.1.
I have attached the hot fix to this response, see the file.
Best Regards,
Marek Neuzil
Hello,
Thank you for reporting of this defect. It is a bug in the AsynchroSerial.drv driver (incorrect include file is used). I have reported this issue to the responsible Processor Expert development team. There should be a hot fix provided soon.
Best Regards,
Marek Neuzil
Hello Tim,
thank you for posting the problem.
can you please send us the KDS demo project and error screenshot? I will check the problem directly on my side. thanks!
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------