Hi Ahmet
Yes, but it is only supported with SDK 1.3. You need to install the Eclipse update for full board and SDK support in KDS.
Go to Help->install new software->Add->Archive and select the update from the <sdk_1.3>\tools\eclipse_update
Hope this information helps you
Have a great day,
Jorge Alcala
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ahmet
Yes, but it is only supported with SDK 1.3. You need to install the Eclipse update for full board and SDK support in KDS.
Go to Help->install new software->Add->Archive and select the update from the <sdk_1.3>\tools\eclipse_update
Hope this information helps you
Have a great day,
Jorge Alcala
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I downloaded Kinetis SDK 1.3.0 Mainline and Go to Help->install new software->Add->Archive and select the update from the <sdk_1.3>\tools\eclipse_update as you indicated and now under Kinetis 1.X Project or PE Project I can see all boards.
But even if i can start a processor expert project with kl27z now if i choose a pe component like BitIO it says this component is not supported for this mcu. And previously where i was able to do this for kl26z now it cannot be used either i think their support is dropped
Hi Ahmet
Yes, as my colleague Erich mentioned PE support has stopped for new parts. So the only way that you can use PE in KL27Z is with SDK components, which does not included components like BitIO.
Best Regards
Jorge Alcala
Yes, PE support has stopped for new parts.
There is way to have some level of Processor Expert for new parts with the Kinetis SDK v2.0, see for example
I plan to write an article about that approach if there is interest. Basically it is using another device (e.g. KL25Z) to generate code for KL27Z.
Erich