Does anyone have a CAD Library part for the MKL27256VFT4?
I hate to have to make my own development board.
Currently, I installed the Autodesk Eagle PCB Version 8.0.1 package.
Or recommend a development board?
The FRDM-KL27Z only has the 64K part on it, which doesn't even do the D/A function.
Thanks in advance,
Ben
已解决! 转到解答。
Thanks Alice,
The need is for a 256K part, so a MKL26 will not work.
Ended up getting a KL27Z256VLH4 part from the Arrow FAE (within a few days even) and replaced it with
the KL27Z64VLH4 part on the FRDM-KL27Z board.
This gives me a dev board with 256K program space and a D/A.
Regards,
Ben
Hello Ben,
Sorry there is demo board for MKL27256VFT4 .
While you can check the FRDM-KL26 board , does its feature can meet your requirement?
FRDM-KL26Z|Freedom Development Platform|Kinetis MCU|NXP
Hope it can helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Alice,
The need is for a 256K part, so a MKL26 will not work.
Ended up getting a KL27Z256VLH4 part from the Arrow FAE (within a few days even) and replaced it with
the KL27Z64VLH4 part on the FRDM-KL27Z board.
This gives me a dev board with 256K program space and a D/A.
Regards,
Ben