In need of a MKL27256VFT4 dev board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

In need of a MKL27256VFT4 dev board

跳至解决方案
1,078 次查看
benmccormick
Contributor III

Does anyone have a CAD Library part for the MKL27256VFT4?

I hate to have to make my own development board.

Currently, I installed the Autodesk  Eagle PCB Version 8.0.1 package.

Or recommend a development board?

The FRDM-KL27Z only has the 64K part on it, which doesn't even do the D/A function.

Thanks in advance,

 Ben

标签 (1)
0 项奖励
回复
1 解答
1,003 次查看
benmccormick
Contributor III

Thanks Alice,

 The need is for a 256K part, so a MKL26 will not work.

 Ended up getting a KL27Z256VLH4 part from the Arrow FAE (within a few days even) and replaced it with

the KL27Z64VLH4 part on the FRDM-KL27Z board.

 This gives me a dev board with 256K program space and a D/A.

Regards,

 Ben

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,003 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ben,

Sorry there is demo board for MKL27256VFT4 .

While you can check the FRDM-KL26 board , does its feature  can meet your requirement?

FRDM-KL26Z|Freedom Development Platform|Kinetis MCU|NXP 

Hope it can helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,004 次查看
benmccormick
Contributor III

Thanks Alice,

 The need is for a 256K part, so a MKL26 will not work.

 Ended up getting a KL27Z256VLH4 part from the Arrow FAE (within a few days even) and replaced it with

the KL27Z64VLH4 part on the FRDM-KL27Z board.

 This gives me a dev board with 256K program space and a D/A.

Regards,

 Ben

0 项奖励
回复