In need of a MKL27256VFT4 dev board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In need of a MKL27256VFT4 dev board

ソリューションへジャンプ
1,090件の閲覧回数
benmccormick
Contributor III

Does anyone have a CAD Library part for the MKL27256VFT4?

I hate to have to make my own development board.

Currently, I installed the Autodesk  Eagle PCB Version 8.0.1 package.

Or recommend a development board?

The FRDM-KL27Z only has the 64K part on it, which doesn't even do the D/A function.

Thanks in advance,

 Ben

ラベル(1)
0 件の賞賛
返信
1 解決策
1,015件の閲覧回数
benmccormick
Contributor III

Thanks Alice,

 The need is for a 256K part, so a MKL26 will not work.

 Ended up getting a KL27Z256VLH4 part from the Arrow FAE (within a few days even) and replaced it with

the KL27Z64VLH4 part on the FRDM-KL27Z board.

 This gives me a dev board with 256K program space and a D/A.

Regards,

 Ben

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,015件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ben,

Sorry there is demo board for MKL27256VFT4 .

While you can check the FRDM-KL26 board , does its feature  can meet your requirement?

FRDM-KL26Z|Freedom Development Platform|Kinetis MCU|NXP 

Hope it can helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,016件の閲覧回数
benmccormick
Contributor III

Thanks Alice,

 The need is for a 256K part, so a MKL26 will not work.

 Ended up getting a KL27Z256VLH4 part from the Arrow FAE (within a few days even) and replaced it with

the KL27Z64VLH4 part on the FRDM-KL27Z board.

 This gives me a dev board with 256K program space and a D/A.

Regards,

 Ben

0 件の賞賛
返信