I've read everything I could find here, and a bunch elsewhere on the web, about how to debug FRDM-K64F code over its USB interface, to no avail. Somewhere I read that you're supposed to use the "GDB OpenOCD Debugging" choice in the Debug Configuration dialog. Initially, I got a popup saying "Error in services launch sequence. OpenOCD requires some -c or -f configuration options to start." Somewhere else I found an explanation that I needed to add "-f kinetis.cfg" to the Debugger config options. Now it doesn't pop anything up, but it fails to load anyway. Instead, the OpenOCD console shows the following messages:
Open On-Chip Debugger 0.8.0-dev-dirty (2014-08-20-11:07)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'cmsis-dap'
Error: unable to open CMSIS-DAP device
Error: unable to init CMSIS-DAP driver
Error: Error selecting 'cmsis-dap' as transport
Runtime Error: C:/Freescale/KDS_1.1.1/openocd/bin/..//scripts/kinetis.cfg:3:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file "C:/Freescale/KDS_1.1.1/openocd/bin/..//scripts/kinetis.cfg", line 3
So I'm stumped. The FRDM users guide says nothing about how to debug. Is there some app note somewhere that I've missed? What do I do next?
已解决! 转到解答。
Hi Bilal,
do you have the latest firmware loaded on the board? See http://developer.mbed.org/handbook/Firmware-FRDM-K64F
But in any case I don't recommend to use the mbed firmware: the Segger and P&E one are much more stable and easier to use.
And 20 times faster!
See http://mcuoneclipse.com/2014/04/27/segger-j-link-firmware-for-opensdav2/
Erich
Just opened up my K64FRDM board and watched the first video and then selected the default debugger and also got the same errors.
Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'cmsis-dap'
Error: unable to open CMSIS-DAP device
Error: unable to init CMSIS-DAP driver
Error: Error selecting 'cmsis-dap' as transport
Runtime Error: C:/Freescale/KDS_3.0.0/openocd/bin/..//scripts/kinetis.cfg:3:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file "C:/Freescale/KDS_3.0.0/openocd/bin/..//scripts/kinetis.cfg", line 3
Pretty disappointing that it does this straight out of the box.
I reflashed the board to use the Segger debugger and it worked no problem,
But still it would be nice to know why the original debugger fails like this.
Hello Paul:
Just checking. Did you manage to connect to your FRDM-K64F?
Tobias has good suggestions there. Personally I had good results with the Segger J-Link firmware.
Regards!
Jorge Gonzalez
I have a Multilink Universal FX, which works fine. At the time I asked, it was elsewhere, but now that I have it, I don't need to get the OpenOCD port working. I used that on a K70 board, and it was pretty slow anyway.
Hi
I have the same problem, may be you guys can help. I have followed the user guide (KDSUG.pdf) and configure the debugger as shown in the image:
When debug, I got the following error:
Note that I am using Ubuntu 14.04 and I am using the preinstalled bootloader. The Debug port is /dev/ttyACM0. I have been searching on the web but could not find any solution to solve this problem. Will look forward for your help in this regard.
Bilal
Hi Bilal,
do you have the latest firmware loaded on the board? See http://developer.mbed.org/handbook/Firmware-FRDM-K64F
But in any case I don't recommend to use the mbed firmware: the Segger and P&E one are much more stable and easier to use.
And 20 times faster!
See http://mcuoneclipse.com/2014/04/27/segger-j-link-firmware-for-opensdav2/
Erich
But what if I'm using the board for mbed applications? Would I still be able to easily flash .bin files to the board if I use a different firmware package? I assume drag-n-drop won't be available.
Hello,
It appeared the same problem for me: error info comes to console as reported in the top of this discussion.
Also the reset red led stays on all the time.
I have updated the firmware as instructed, trying both alternatives PEMicro and Segger J-Link, but didn't change the situation.
Could you please advice if the reset led always on would point to different problem/solution ?
Regards,
Adrian
Hello Paul DeRocco,
debugging with the preinstalled bootloader does not seem to work.
But here are some links that explain how you can replace it by the PEMicro or Segger J-Link:
https://community.freescale.com/docs/DOC-100733
https://community.freescale.com/docs/DOC-100705
http://mcuoneclipse.com/2014/04/27/segger-j-link-firmware-for-opensdav2/
http://www.segger.com/opensda.html
Regards,
Tobi