Dear Sir/Mam,

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dear Sir/Mam,

1,912件の閲覧回数
karanchaudhary
Contributor I

Dear All,

 

This is my first time when i am using 32 bit and freescale controller.

Kindly mail me sample code workspace  for 1 sec delay using FTM2.

Mail ID - karan.atepower@gmail.com

 

Regards,

Karan Chaudhary

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

1,242件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Karan,

Thank for your interesting about our product.

Please tell me which chip do you use ? And also which IDE ?

BR

Alice

0 件の賞賛
返信

1,242件の閲覧回数
karanchaudhary
Contributor I

Dear Sir/Mam,

I am using Kinetics KEA8 micro controller and ide is Code warrior 10.6.4

Please reply as soon as possible.

Regards !

Karan Chaudhary,

(ATE Power Connection Pvt. Ltd.)

Mob : + 91 - 8860194660.

On Thu, Jan 7, 2016 at 3:23 PM, Alice_Yang <admin@community.freescale.com>

0 件の賞賛
返信

1,242件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Karan,

There is no the FTM delay demo function on the NXP official website, so i crate one demo by myself.

I use the CW10.6.4, TRK-KEA8,  please the attachment .

** ###################################################################

this function delay t ms

** ###################################################################

*/

void delayms(int t)

{

    EventCount = 0;

  

    while(t > EventCount);

}

In this project , define the period of the FTM interrupt to 1ms , then the "EnventCount" will be add 1

when it run to the interrupt.

I think you can refer to this create one delay function on your project .

0 件の賞賛
返信

1,242件の閲覧回数
karanchaudhary
Contributor I

Dear Alice,

*Its my starting on 32 bit controller so i am unable to generate *

FTM interrupt for timer delay. I know the logic you told but

my problem is to generate interrupt for FTM2.

I am using TRK-KEA8 evaluation board.

Thanks for your revert.

Regards !

Karan Chaudhary,

(ATE Power Connection Pvt. Ltd.)

Mob : + 91 - 8860194660.

On Fri, Jan 8, 2016 at 1:01 PM, Alice_Yang <admin@community.freescale.com>

0 件の賞賛
返信

1,242件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Karan ,

THe demo i send you is just for the board TRK-KEA8, you can directly use it .

BR

Alice

0 件の賞賛
返信

1,242件の閲覧回数
karanchaudhary
Contributor I

Hello Alice,

Thanks a lot for revert.

Can i have sample code for input capture for the same board.

Regards !

Karan Chaudhary,

(ATE Power Connection Pvt. Ltd.)

Mob : + 91 - 8860194660.

On Tue, Jan 12, 2016 at 3:56 PM, Alice_Yang <admin@community.freescale.com>

0 件の賞賛
返信

1,242件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Karan,

In the Typical Usage , there is a demo about input capture, you can refer to it .

Please right click the component , the select the "help on component", the refer to the demo of "

"

pastedImage_1.png

pastedImage_0.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信