After about 5 mins of being plugged into the battery, the drone (ESCs/motors I believe) start beeping constantly and won't stop. Any solutions?
解決済! 解決策の投稿を見る。
This beeping is from the ESCs when they have not received an input for a while. This is part of a failsafe and protection from leaving a drone powered on in the field. When working at the desktop you can just unplug the power connector between the PDB (Power distribution board) and the Power module. So no power to the ESCs. Keep the power connection from Battery ->powermodule->FMU.
This beeping is from the ESCs when they have not received an input for a while. This is part of a failsafe and protection from leaving a drone powered on in the field. When working at the desktop you can just unplug the power connector between the PDB (Power distribution board) and the Power module. So no power to the ESCs. Keep the power connection from Battery ->powermodule->FMU.