Why are the drone motors beeping?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why are the drone motors beeping?

Jump to solution
2,969 Views
nxf58541
NXP Employee
NXP Employee

After about 5 mins of being plugged into the battery, the drone (ESCs/motors I believe) start beeping constantly and won't stop. Any solutions?

0 Kudos
1 Solution
2,911 Views
nxf58541
NXP Employee
NXP Employee

This beeping is from the ESCs when they have not received an input for a while. This is part of a failsafe and protection from leaving a drone powered on in the field. When working at the desktop you can just unplug the power connector between the PDB (Power distribution board) and the Power module. So no power to the ESCs. Keep the power connection from Battery ->powermodule->FMU. 

View solution in original post

0 Kudos
1 Reply
2,912 Views
nxf58541
NXP Employee
NXP Employee

This beeping is from the ESCs when they have not received an input for a while. This is part of a failsafe and protection from leaving a drone powered on in the field. When working at the desktop you can just unplug the power connector between the PDB (Power distribution board) and the Power module. So no power to the ESCs. Keep the power connection from Battery ->powermodule->FMU. 

0 Kudos