What battery should I use with the HoverGames drone? 3S or 4S?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What battery should I use with the HoverGames drone? 3S or 4S?

Jump to solution
1,886 Views
nxf58541
NXP Employee
NXP Employee

Have any of you been using a 4S battery? I've been using one of my 3S 2200mAh battery I had around from my smaller quads but thinking of getting a higher capacity 4s. Any suggestions?

0 Kudos
Reply
1 Solution
1,853 Views
nxf58541
NXP Employee
NXP Employee

3S 2200mAh will not last very long, you should probably upgrade to a 4000mAh+ capacity battery. I have used both 3S 5200 mAh and 4S 5200 mAh batteries with the HoverGames drone kit. Also keep in mind the discharge rating. For 2200mAh batteries you probably need at least 30C to be safe, but for 5200 mAh a 15C rating is enough. There are some recommended battery specifications on this page: https://nxp.gitbook.io/hovergames/userguide/getting-started/not-included-items#lipo-battery-specific....

View solution in original post

1 Reply
1,854 Views
nxf58541
NXP Employee
NXP Employee

3S 2200mAh will not last very long, you should probably upgrade to a 4000mAh+ capacity battery. I have used both 3S 5200 mAh and 4S 5200 mAh batteries with the HoverGames drone kit. Also keep in mind the discharge rating. For 2200mAh batteries you probably need at least 30C to be safe, but for 5200 mAh a 15C rating is enough. There are some recommended battery specifications on this page: https://nxp.gitbook.io/hovergames/userguide/getting-started/not-included-items#lipo-battery-specific....