I'm having a problem with my ESC or Motor. What should I do?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I'm having a problem with my ESC or Motor. What should I do?

Jump to solution
2,044 Views
nxf58541
NXP Employee
NXP Employee

Need some troubleshooting help. I have a motor that spins fine without the propeller on it, but will not spin once I put the weight of the propeller on it. I installed a new motor at that location and the new motor has the same behavior. I've checked all the connections on the ESC and power distribution panel and can't find anything wrong.

0 Kudos
Reply
1 Solution
1,973 Views
nxf58541
NXP Employee
NXP Employee

If you think it's the ESC, which it sounds like it may be, NXP will do an RMA for just that part. 

View solution in original post

0 Kudos
Reply
1 Reply
1,974 Views
nxf58541
NXP Employee
NXP Employee

If you think it's the ESC, which it sounds like it may be, NXP will do an RMA for just that part. 

0 Kudos
Reply