I'm having a problem with my ESC or Motor. What should I do?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm having a problem with my ESC or Motor. What should I do?

ソリューションへジャンプ
1,909件の閲覧回数
nxf58541
NXP Employee
NXP Employee

Need some troubleshooting help. I have a motor that spins fine without the propeller on it, but will not spin once I put the weight of the propeller on it. I installed a new motor at that location and the new motor has the same behavior. I've checked all the connections on the ESC and power distribution panel and can't find anything wrong.

0 件の賞賛
返信
1 解決策
1,838件の閲覧回数
nxf58541
NXP Employee
NXP Employee

If you think it's the ESC, which it sounds like it may be, NXP will do an RMA for just that part. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,839件の閲覧回数
nxf58541
NXP Employee
NXP Employee

If you think it's the ESC, which it sounds like it may be, NXP will do an RMA for just that part. 

0 件の賞賛
返信