1. See the pic. When I trying to generate code for the button with cyrillic text (and some other widgets) the TypeError appears. What is wrong here?
2. When 'Generate Fonts' command is executed, this happens for ALL characters instead of a subset which entering by the user in 'Word' field. How to generate the only used font characters?
已解决! 转到解答。
Hello brendon
The shared project works well in V1.3.1, Please use the latest version to try. @vladi552
Thanks
Liubin
1. The export fonts code file name: must be the same as the fonts file name in the "projectPath/generated/guider_fonts".
2. This is the font size you use when designing your UI by the GUI guider.
3. Select the "4 bit-per-pixel".
4. Select the font file
5. Input your used text.
6. Click the button and download the generated fonts file.
a). The current 1.3.0 version does not support the input of such characters, we plan to support 1.3.1 in March.
b). This is a workaround.
1. Please design UI with English characters instead of Russian characters.
2. To generated Russian characters by this link fontconverter.
3. Use this fonts C file ("lv_font_Montserrat_SemiBold_19.c") to replace "test\generated\guider_fonts\lv_font_Montserrat_SemiBold_19.c"
4. Modify the "test\generated\setup_scr_screen.c" like the sip
5. Execute "make -r && make -r run" on this "test\lvgl-simulator" path.
This is my first project in GuiGuider. It looks like the character codes above U+0x00FF is not supported. If the users enter this kind of characters Type error appears and resulted С code cannot be generated...