X-Y plots: possibly a feature request

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

X-Y plots: possibly a feature request

ソリューションへジャンプ
3,860件の閲覧回数
martin_reszat
Contributor I

Hi FreeMASTER team,

first of all let me tell you that for me FreeMASTER is high up there, along with sliced bread and velcro shoes :-). Thank you for all the effort that went into this indispensable tool!

After years of successful use, today I finally get around to ask for a feature (or maybe just a pointer?). I can't seem to find the "ideal" settings for a common scenario: plotting, say, motor phase voltages and currents against rotor angle over a number of revolutions (see attached files).

Is there already a way to suppress the "retrace" lines, which totally spoil the nice "spline" feature in this scenario, unless you use the recorder and fiddle with buffer depth and trigger points until you see just one revolution? Or maybe there's an option I don't know of to make the "points" actual pixel-sized dots, at least smaller than they are right now?

If not, a new feature would allow to suppress line/spline calculation based on the X-variable slope in the time domain.

    

 

 

0 件の賞賛
返信
1 解決策
3,816件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Martin,

thanks for your inputs. Both are good ideas.

I agree that today the X-Y line-type graph is only good for continuous functions at the X axis (e.g drawing Lissajous figures). Adding a line break when negative delta is detected on in the X series should be quite easy and useful for use-cases like yours. Also, we'll look at the "point" size settings.

Thanks,
Michal

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,802件の閲覧回数
martin_reszat
Contributor I

Hello Michal,

thank you for your reply. I'm looking forward to seeing a great tool getting even bettter.

Regards,

Martin

0 件の賞賛
返信
3,150件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Dear Martin,

the line-breaking feature in X-Y graph has just been released in version 3.2.3. If you spot any issue, please create a new question/thread in this forum.

Thanks,
Michal

 

0 件の賞賛
返信
3,817件の閲覧回数
MichalH
NXP Apps Support
NXP Apps Support

Hello Martin,

thanks for your inputs. Both are good ideas.

I agree that today the X-Y line-type graph is only good for continuous functions at the X axis (e.g drawing Lissajous figures). Adding a line break when negative delta is detected on in the X series should be quite easy and useful for use-cases like yours. Also, we'll look at the "point" size settings.

Thanks,
Michal

0 件の賞賛
返信