Hi,
I am using Windows 11, 64 bit PC powered by AMD Ryzen7 processor.
I am facing a typical error is running freemaster,
- It gives various errors on selection of each window.
- App control page is not visible completely.
- Parameters are not passed in real time to the MCU, every time i have to load the parameters through the debug mode. This makes the tunning a very lengthy process.
Can you kindly help me to use the freemaster in the right way.
Regards,
Akshay
Hello,
first, let's see if FreeMASTER can connect to the target board at all. In project Options, at the HTML tab, please remove the path to the "Control Page". This will remove the GUI from the FreeMASTER and will only keep the variables in the Watch view.
Now, when you press the "GO" button, do you see any variable values or just question marks "?" ?
If you do NOT see any real value, then please try to use a different COM port when connecting or different speed. The Connection Wizard could help you with this.
Please show us any errors you get during connecting to the board.
Thanks,
Michal