Freemaster connect fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Freemaster connect fail

2,276 次查看
814420552
Contributor III

Dear all,

   when i connect  my board with openSDA, then open freeMaster tool,  boautrate is 115200, when click next step, it happeened the following error, pls  help me, only connect board and pc with USB line (openSDA)

pastedImage_1.png

0 项奖励
回复
3 回复数

2,180 次查看
VilemZ
NXP Employee
NXP Employee

Hello,

it looks, that you want to connect via UART instead of the OpenSDA. For connection via UART, you need have the running Freemaster in the board too. 

If you want to use only OpenSDA, please select the highlited option in wizard.

pastedImage_1.png

And after then, you will see options of the debug connections:

pastedImage_2.png

Best regards,

Vilem

0 项奖励
回复

2,180 次查看
814420552
Contributor III

hello, whether has some manual or document for how to use this tool(FreeMaster)? 

wish you can share it to me, thanks very much!!

0 项奖励
回复

2,180 次查看
VilemZ
NXP Employee
NXP Employee

Hello,

you can find all documents on the NXP web page: FreeMASTER Run-Time Debugging Tool | NXP 

Best regards,

Vilem

0 项奖励
回复