Hello, ladies and gentlemen,
i have a problem with FreeMASTER 3.0
I have the installation file under :
downloaded as an installation file for Windows, I also downloaded the required drive files.
After installing the two files I wanted to start FreeMASTER. After several clicks on the icon of the program, nothing happened.
Running the program with administrator rights was also unsuccessful.
Can anyone help me in this matter?
已解决! 转到解答。
Dear Dariusz,
I'm sorry for your troubles. It is indeed quite strange that even the 2.0 does not show up. What is your Windows 10 localization (language)?
Can you please try the following:
Thank you for your patience,
Michal
Dear Dariusz,
can you describe a configuration of your computer? (Windows version and RAM).
Do you have a Chrome browser installed on your computer and does it work fine?
Can you please try to install and run the FreeMASTER 2.0 to see if this version works well?
Thanks,
Michal
Hey, Michal,
the configuration of my computer is the following :
- Windows 10 Enterprise as operating system
- 64-bit operating system, x64-based processor
- RAM = 8 GB
I have tried to install version 2.0. The installation location was successful, but the result remains the same as with the other versions (2.5 and 3.0). The program does not start.
Yes, Google Chrome is installed on my computer and it works fine.
Regards Dariusz
Dear Dariusz,
I'm sorry for your troubles. It is indeed quite strange that even the 2.0 does not show up. What is your Windows 10 localization (language)?
Can you please try the following:
Thank you for your patience,
Michal
Hay Michal,
the operating system runs with German language.
I tried the first variant and it worked.
I deleted all entries under HKEY_CURRENT_USER\Software\Freescale\FreeMASTER.
The software went on.
Thank you very much.