HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1

跳至解决方案
889 次查看
vivek5676
Contributor II

Hi,

We am using i.mx9352 A1 model.

we are unable to port the BSP file due to some error is coming as given below

=======================================================

Success 0 Failure 1

 


1:2 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -f imx-boot-imx93evk-sd.bin-flash_singleboot

=============================================================================

Could you provide solution for that error

Thanks,

Vivek

 

0 项奖励
回复
1 解答
844 次查看
vivek5676
Contributor II

My problem get resolved after changes done in hardware.  

在原帖中查看解决方案

0 项奖励
回复
3 回复数
727 次查看
Binh_Hoang
Contributor II

Hi @vivek5676,

I'm facing the same issue. Could you please let me know which change is needed for this case? Please give me more details. 

Thank you in advance,

Binh

0 项奖励
回复
641 次查看
vivek5676
Contributor II

Hi @Binh_Hoang 

Kindly check the voltage as per Table 29 of NXP hardware design guide and check  the VDD_SOC_0V8 at SOC end.

Thanks

845 次查看
vivek5676
Contributor II

My problem get resolved after changes done in hardware.  

0 项奖励
回复