HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1

ソリューションへジャンプ
667件の閲覧回数
vivek5676
Contributor II

Hi,

We am using i.mx9352 A1 model.

we are unable to port the BSP file due to some error is coming as given below

=======================================================

Success 0 Failure 1

 


1:2 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -f imx-boot-imx93evk-sd.bin-flash_singleboot

=============================================================================

Could you provide solution for that error

Thanks,

Vivek

 

0 件の賞賛
返信
1 解決策
622件の閲覧回数
vivek5676
Contributor II

My problem get resolved after changes done in hardware.  

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
505件の閲覧回数
Binh_Hoang
Contributor II

Hi @vivek5676,

I'm facing the same issue. Could you please let me know which change is needed for this case? Please give me more details. 

Thank you in advance,

Binh

0 件の賞賛
返信
419件の閲覧回数
vivek5676
Contributor II

Hi @Binh_Hoang 

Kindly check the voltage as per Table 29 of NXP hardware design guide and check  the VDD_SOC_0V8 at SOC end.

Thanks

0 件の賞賛
返信
623件の閲覧回数
vivek5676
Contributor II

My problem get resolved after changes done in hardware.  

0 件の賞賛
返信