problem with MCF5208 interfacing with 64M 16-bit Width SDR SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with MCF5208 interfacing with 64M 16-bit Width SDR SDRAM

2,198件の閲覧回数
kuoching
Contributor I
i try to develop a board using MCF5208 and ISSI IS42S16400(64M-bit,16bit width SDRAM).
I found a very strange issue :
when i  try to change a data in the SDR ,another address will changes accordingly.
The address is the current address + 256
for example,
When I write a 0x0002 to 0x40000000,   the  data at 0x40000200 will change to 0x0002
my schmatics follows the illustration on Page 317 Figure 8-2 of MCF5208RM.
 
Your help will be highly appriecated .
 
 
Thanks a lot 
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,210件の閲覧回数
Edison_Tran
Contributor I

Hi Kuoching

 

Have you found the solution for this problem ? I'm facing the same problem and hope you can help with your past experiences

 

Thanks,

Edison

0 件の賞賛
返信