MCF52233CAF60 and monitoring my power supplies

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52233CAF60 and monitoring my power supplies

1,592件の閲覧回数
rlstraney
Contributor III

Hello,

I have two +5 volt power supplies in my product.  One is used as a redundant supply so only one is active at a time.  I want to report to the user via my command line the status of the power supplies.   

 

I really only need to report if they are "up" - not necessarily their exact voltages.  

 

Can anyone share how this is generally done? 

 

Here are my first ideas:

 

Use 2 voltage supervisors to monitor each supply and run their outputs to my 52233 and just read the pins for the correct logic level. 

 

I also thought of running the voltages from the supplies over to the processors A/D inputs (Via a voltage divider since it appears the 52233 can read up to Vrefh which cannot exceed VDDA.) and sampling them.

 

Or are there other ways to accomplish this? 

 

Thanks

Renee

ラベル(1)
0 件の賞賛
返信
1 返信

1,046件の閲覧回数
admin
Specialist II

rlstraney wrote:
Or are there other ways to accomplish this?
 

You could simply connect them to digital inputs using suitable voltage dividers. Information on digital input switching threshold levels should be in the datasheet.

If you want a more or less precise comparator, have a look at TL431A. It's extremely cheap and should be good for this job.

0 件の賞賛
返信