Coldfire V2 MCU M5225x family launched today

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coldfire V2 MCU M5225x family launched today

1,799 Views
mjbcswitzerland
Specialist V
Hi All

Today freescale launched their new Coldfire processor family (single chip V2 MCU):

Featuring Ethernet + USB+ CAN + Flexbus + encryption-functions, with up to 64k SRAM and 512k FLASH.

Further links, details and demos are available here:
http://www.utasker.com/forum/index.php?topic=499.0


Regards

Mark

www.uTasker.com



Message Edited by mjbcswitzerland on 2009-01-22 10:46 PM

Message Edited by rav on 2009-01-22 11:43 PM
Labels (1)
0 Kudos
Reply
3 Replies

528 Views
TomFreescale
Contributor I
Hi Mark,

This looks like a good part. Any idea how does the MQX software compare to uTasker?


0 Kudos
Reply

528 Views
mjbcswitzerland
Specialist V
Hi Tom

I think that the best way to find out is to give them both a try. Each one will have its own advantages and disadvantages - as everything in life.

The uTasker is unique in its real-time device simulator. If it includes the features required for a particular project it will generally enable shortest time-to-market and smallest memory size compared to most other alternatives.

Try a small project, see which is easiest to use, ask questions when something is not clear, see which runs best and compare code sizes, and find out which you would be most comfortable with for the next serious job....

Good luck

Regards

Mark

www.uTasker.com

0 Kudos
Reply

528 Views
Nouchi
Senior Contributor II
Hi,

I would named this family the "missing link" :smileyvery-happy:


Emmanuel.
0 Kudos
Reply