What's the matter with the COP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What's the matter with the COP?

1,992 次查看
wangbo
Contributor I
I design a board with MPC8548E,and design the JTAG interface as the MPC8548EEC suggested,when I used the codewarrier to connect the board,it is failed and report " cannot reset the targets",if not chose the "Reset target On launch",it can connect to the board.I check out the signal "HRESET",and find it is asserted at the end of the process.my codewarrier and simulator all work well.so what's wrong with my board,thx.
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

585 次查看
genuap
NXP Employee
NXP Employee
Have you looked at JTAG TRST? This should be ANDED with POR. I believe there's a diagram in the HW spec or checklist that shows how to do this.
0 项奖励
回复

585 次查看
wangbo
Contributor I
yes,I'm sure that TRST is ANDED with POR.I compare it to a 8349 board,and find that TRST on 8349board is pull down by a 1k res,and the 8548e HW SPEC do not use any pull up or pull down res,is it correct?
0 项奖励
回复