T2080 CodeWarrior Connetion Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 CodeWarrior Connetion Problem

1,510件の閲覧回数
tomsaluzzo
Contributor III

Trying to connect CodeWarrior to customer hardware.Get the following error:

 

Launching T2080_ADP-core00_RAM_T2080_Connect' has encountered a problem. Would you like to export diagnostic information and send it to Freescale?

 

Error launching T2080_ADP-core00_RAM_T2080_Connect

 

Error launching T2080_ADP-core00_RAM_T2080_Connect

     CCSProtocolPlugin : Failed to correctly configure the JTAG chain

 

 

Could it be possible that since I have two devices in my JTAG chain that I have to tell codewarrior how many shifts it needs to make to talk to the T2080? Are there instructions on how to do that?

ラベル(1)
0 件の賞賛
返信
1 返信

1,102件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Tom Saluzzo,


It is possible to use CW JTAG configuration file to specify multiple device on a JTAG chain, you could use the processor name directly in JTAG oonfig file for details, please refer to "Using a JTAG configuration file to specify multiple linked devices on a JTAG chain" in CW_PA_v10.4.0\PA\Help\PDF\Targeting_PA_Processors.pdf.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信