How much size is required for download algorithm in code warrior hardware diagnostic tool?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How much size is required for download algorithm in code warrior hardware diagnostic tool?

跳至解决方案
806 次查看
karunakaranradh
Contributor IV

Hi,

 

I am planning to use the inbuilt 512KB SDRAM of T2080 as a target CPU in code warrior hardware diagnostic tool.

 

How much memory is required to download the algorithm to run the hardware diagnostic tool?

 

Regards

Karunakaran R

标签 (1)
1 解答
547 次查看
addiyi
NXP Employee
NXP Employee

The flash programmer algorithm required a maximum 30k.

Adrian

在原帖中查看解决方案

2 回复数
548 次查看
addiyi
NXP Employee
NXP Employee

The flash programmer algorithm required a maximum 30k.

Adrian

547 次查看
karunakaranradh
Contributor IV

Hi Adrain,

I configured the SDRAM in code warrior script  and set the SDRAM address as download algorithm address. With is configuration, i performed the 256MB of DDR3 memory test. it was working fine and faster also when compare with DDR3 set as download algorithm.

Thanks for your information.

Regards

Karunakaran R

0 项奖励
回复