Eval License for CW10 or CW8.1?? (MPC555)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eval License for CW10 or CW8.1?? (MPC555)

Jump to solution
2,717 Views
Mr_Freez
Contributor II

Hi

I recently downloaded the eval version of Codewarrior 8.1 for the MPC555.  This was the pre-eclipse version that only ran on Windows XP.

I was just granted an extension to the license by Freescale support.  However when I replace the old license I still  get an error that the license is invalid.  I am wondering if the license extension is for the Eclipse based tool? or ??

The support person said that if I purchased the tool I would need to get the Professional version to get support for the MPC555.  When I look for this version I still end up at the same eval download???

 

Confused

Rich

Labels (1)
0 Kudos
Reply
1 Solution
573 Views
CrasyCat
Specialist III

Hello

 

CodeWarrior for PA5xx has not been ported to eclipse yet.

 

Can you please add following line at the beginning of your license.dat file.

 

  FEATURE Win32_CWIDE_Limited metrowks 5.5 permanent uncounted 2589EF7E8174 HOSTID=ANY

 

That should at least allow you to start the IDE.

 

Then check if you can build. If this does not work the system should return some message explaining what is going on.

 

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
574 Views
CrasyCat
Specialist III

Hello

 

CodeWarrior for PA5xx has not been ported to eclipse yet.

 

Can you please add following line at the beginning of your license.dat file.

 

  FEATURE Win32_CWIDE_Limited metrowks 5.5 permanent uncounted 2589EF7E8174 HOSTID=ANY

 

That should at least allow you to start the IDE.

 

Then check if you can build. If this does not work the system should return some message explaining what is going on.

 

CrasyCat

0 Kudos
Reply
573 Views
Mr_Freez
Contributor II

Thanks Crasy Cat...will try that

0 Kudos
Reply