Hi Wang,
I am using customized Lx2160aQDS processor, and 2 Discrete RAM (DDR4) is used with size of 4GB each.
32bit width of speed support 1300Mtps - 3200Mtps
Regards,
Arunwilliam S
I confirmed that QCVS does not work with RDIMM on LX2160ARDB. Also there is no QCVS support available.
Hi Wang,
I am using customized Lx2160aQDS processor, and 2 Discrete RAM (DDR4) is used with size of 4GB each. 32bit width of speed support 1300Mtps - 3200Mtps
Regards, Arunwilliam S
Have you passed DDR validation with QCVS DDRv tool?
Would you please provide your screenshot of your QCVS DDRv tool.
First after creating a QCVS DDR project, please fill DDR parameters in "Properties" panel according to your DDR datasheet.
Then select all the 3 items under "Validation stage" to do DDR validation first. After these validations passing, you could do "Operational DDR test".
If your problem persists, please capture your CCS console log to me to do more investigation.
After click "Start Validation", CodeWarrior Connection Sever(CCS) will pop up at the right bottom of the Windows task bar, please double click and open it, then type "log v" and click "Start Validation” again, the low level CCS log will be printed in the console, please capture the whole CCS log to me to do more investigation.
DDR Tool has to be used with non-hardcoded RCW option - i.e. valid RCW has to be present in the RCW source Flash.
In QCVS DDR project, in "Connections View" panel, please click "Re-check connection" button to check whether "This connection is working".
Hi wang,
wang: DDR Tool has to be used with non-hardcoded RCW option - i.e. valid RCW has to be present in the RCW source Flash
Arun : Yes, I have used non-hardcoded RCW, logs are attached.
DDR4 : 2600MHz
Wang: In QCVS DDR project, in "Connections View" panel, please click "Re-check connection" button to check whether "This connection is working".
Arun: Yes, This connection is working , when I do Re-check option from Connection View panel
Discussing with the AE team.
Hi wang,
Any update ?
Sorry for the late reply.
The expert in the AE team is out of office previously, I have contacted them again, will provide more update as soon as possible.
Please refer to the following feedback from the AE team.
Please clarify what is the inquiry.
Is the customer system is working at 2600MT/s when using atf/uboot? and when you try to run the same board using QCVS tools is failing?
If that is the inquiry then please provide more details on how is the QCVS configured? using import from target?
What other options have you tried?
After configuration wizard is completed go directly to run a functional test. and provide the log from QCVS.
Still waiting for the feedback from the AE team, I will contact them again.
Hi Wang,
Any update?