About usbtap used on mpc8241 board problem-help me!!!!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About usbtap used on mpc8241 board problem-help me!!!!!!

1,337件の閲覧回数
K6Dwmv
Contributor I
I'm now having a problem where I can only see 1/2 of my SDRAM.
My board cpu is mpc8241 and mpc8241 have 32bit data bus connected to sdram that is composed of two 16bit  width data bus chips.I try to use codewarrior and usbtap to connect this board and find  can only see 1/2 of my SDRAM,what is the reason  of phenomenon? I can sure the initialization files is connect.
 
In this forum,i find a guy had ecounted the same prolem as me ,but no answer.
whether is the data  width that usbtap access to cpu though JTAG at a time  is eight???? Please give me answer,
 
Address       data     
00000000   749e8778 00000000 7cdc3378 00000000
00000010   3B000000 00000000 480037DD 00000000
 
Can usbtap support 32bit width data bus of sdram????? I have spended a lot of time to find out the solution,but i fail ,please help ,thanks!!!
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

400件の閲覧回数
Voxan
Contributor III
Hi K6Dwmv,

I would recommand to contact the support line, details can be founded here:
http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=054670&tid=FSH

Create a Service Request at: "Submit a service request" you should have a FSL account to access this page though.

Now regarding your request, the closest  supported PQ2 into CW is 8245, if you create a dummy project through the project wizard, you'll see it is using the "Sandpoint_init.cfg" and the "Sandpoint.mem" files. I would recommand to use those first... if it does not do the trick, please submit an SR.

Hope this helps...

Regards
0 件の賞賛
返信