Why is file debugout.txt being created?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why is file debugout.txt being created?

跳至解决方案
1,941 次查看
frankbaird
Contributor III


I recently upgraded from CW 10.6.3 to 10.6.4 and now, every time I debug my program, the file debugout.txt is created at the top level of my workspace. Despite it being called a text file, it is clearly a binary file. Why is this file being created, and how do I stop it? If I can't stop it, how do I at least read and interpret it?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,815 次查看
BlackNight
NXP Employee
NXP Employee

Hi Frank,

could it be that you are using semihosting? In that case the target could write that file.

Erich

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,816 次查看
BlackNight
NXP Employee
NXP Employee

Hi Frank,

could it be that you are using semihosting? In that case the target could write that file.

Erich

0 项奖励
回复
1,815 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Fran,

Which chip do you used, could you please take a screenshot about the .txt file place.

Then i will check it .

BR

Alice

0 项奖励
回复
1,815 次查看
frankbaird
Contributor III

I am using the MCF52258 chip. The image below shows the file's location. I have attached the txt file as well.

pastedImage_0.png

0 项奖励
回复
1,815 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Frank,

Is the debugout.txt file created only when debugging that project? Could you share the project so we can reproduce it on our side?

Could you also tell us which programming interface are you using?

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 项奖励
回复