There are 2 evaluation boards for  MC9S08DZ60AMLC. DEMO9S08DZ60 and EVB9S08DZ60. What is difference between these two? which one is better?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

There are 2 evaluation boards for  MC9S08DZ60AMLC. DEMO9S08DZ60 and EVB9S08DZ60. What is difference between these two? which one is better?

561件の閲覧回数
jagrativalecha
Contributor I

I have chosen MC9S08DZ60AMC(32 bit LQFP) for my project. There are 2 evaluation boards available for it. DEMO9S08DZ60 and EVB9S08DZ60. What is difference between the two? Which one is better.

 

Is there any other option for loading program to MCU. I will not be using evaluation board in my project.

ラベル(1)
0 件の賞賛
返信
1 返信

397件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JAGRATI,

"which one is better" depends on user requirement.

DEMO9S08DZ60 is cheaper but EVB9S08DZ60 integrates more user interface.

For more information, see these two urls. they includes the board description and pictures, etc.

S08D Family Demonstration board|NXP 

S08D Family Evaluation Boards|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信