There are 2 evaluation boards for  MC9S08DZ60AMLC. DEMO9S08DZ60 and EVB9S08DZ60. What is difference between these two? which one is better?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There are 2 evaluation boards for  MC9S08DZ60AMLC. DEMO9S08DZ60 and EVB9S08DZ60. What is difference between these two? which one is better?

560 Views
jagrativalecha
Contributor I

I have chosen MC9S08DZ60AMC(32 bit LQFP) for my project. There are 2 evaluation boards available for it. DEMO9S08DZ60 and EVB9S08DZ60. What is difference between the two? Which one is better.

 

Is there any other option for loading program to MCU. I will not be using evaluation board in my project.

Labels (1)
0 Kudos
Reply
1 Reply

396 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi JAGRATI,

"which one is better" depends on user requirement.

DEMO9S08DZ60 is cheaper but EVB9S08DZ60 integrates more user interface.

For more information, see these two urls. they includes the board description and pictures, etc.

S08D Family Demonstration board|NXP 

S08D Family Evaluation Boards|NXP 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply