Pushbutton switch stimulation using the special edition version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pushbutton switch stimulation using the special edition version

Jump to solution
3,463 Views
FC
Contributor III

Hello,

 

Just want to confirm that the special edition does not allow stimulation of a pushbutton or any switch connected to an I\O port.  I can toggle an LED using the graphical tools, but not a switch input.

 

Is there a way to stimulate an input using the special edition version?

 

Thanks

 

FC

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,388 Views
CrasyCat
Specialist III

Hello

 

The Special edition only limits the number of instruments you can add in a visualization tool window.

It does not limit the functionality of the instruments.

 

I did try on a simple project and I can toggle a bit on POTA through a Switch Instrument.

Did you initialize the port direction register appropriately to allow input on that bit?

 

As you did not specify which version of CodeWarrior you are using I assumed you are using CodeWarrior for MCU V6.2.

 

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
2,388 Views
FC
Contributor III

Hello again,

 

I have the read the posts similiar to this topic, but they discuss simulating KBI interrupts.  For a polling application, can a switch component change the input value on a pin?

 

Thanks 

0 Kudos
Reply
2,389 Views
CrasyCat
Specialist III

Hello

 

The Special edition only limits the number of instruments you can add in a visualization tool window.

It does not limit the functionality of the instruments.

 

I did try on a simple project and I can toggle a bit on POTA through a Switch Instrument.

Did you initialize the port direction register appropriately to allow input on that bit?

 

As you did not specify which version of CodeWarrior you are using I assumed you are using CodeWarrior for MCU V6.2.

 

CrasyCat

0 Kudos
Reply