I've just finished installing the newest update to CW 10.5 and now most of the keybuindings and keyboard shortcuts stopped working.
DEL, Ctrl+C, Ctrl+V are the most egregious but there are a certain number of other shortcuts that also no longer work.
Selecting those commands via context menus works.
I've already reset everything to defaults and I've also deleted my workspace and created a new one. Reboot and closing/reopening my projects didn't work either.
Before I spend half of my work day to delete and reinstall CW is there another way to restore keybinds to working order again?
I have windows 64-bit ultimate and codewarrior 10.6, everything up to date. Mmy delete key occasionally stops working just in all things codewarrior related (all other programs work normally). Restart codewarrior and it comes back. Just a little annoying, its only happened twice in several months.
Hi Carl,
I know that this was a problem with the 10.5 update, but I have not seen this or any report on 10.6.
Does the workaround described above
>The only solution is : type anything - > highlight it - .> ctrl-x it - > ctrl-v it. Now all that shortcuts should work
work for you too?
If so, it really could be the same problem, maybe it happens very likely?
Erich
How to install second update to MCU10.5?
using this link? : http://freescale.com/lgfiles/updates/Eclipse/MCU10_5/com.freescale.mcu.updatesite
but what element should be upgraded?
I upgraded PEx (CW for MCU 10.5 PEx Update v1.0.0 -> MCU10.5 PEx CORE UPDATE 1.0.1) and every other packages that I think could have a relation with this problem but Ctrl-c Ctrl-v still dont work.
I would like to use 10.6 instead but I have license only for 10.5.
Could you be more specific about required package?
David
After working for a certain amount of time in CW 10.5 the keybindings suddenly start working again until I close and reopen CW (which I have to do often with 10.5 since it's such a broken mess) then they stop working again
Same here: after upgrade to 10.5 shortcut keys stop working, but sometime later in the session, they seem to start working again...Irritating, isn't it.
I have submitted a service request.
One thought...I'm running CW10.5 on Windows XP. Could the problem be related to that?
- R
I have seen this happen twice on Windows 7 x64 in the last week. I tried everything I could think of and ended up uninstalling and reinstalling. That is the first real problem I have had since 10.5 was released. Developing on Kinetis using the Freescale toolchain, not GCC and it seems to be very stable for me. I found that the GCC toolchain produces much larger code footprint when identical code is compiled with Optimization set to 0.
Pure happenstance, being observant, and having old habits (keeping on trying the Ctl-C and Ctl-V, even when I "knew" they were not working).
Note the "seems to" - I am not entirely sure it will work for everybody.