Is Codewarrior for s12(x) V5.1 support the device(MC9S12XEA256)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is Codewarrior for s12(x) V5.1 support the device(MC9S12XEA256)?

Jump to solution
1,751 Views
whz
Contributor I

I downloaded CWS5.1 from WWW.NXP.COM, but cann't find the device(MC9S12XEA256) when building project,or when choosing "Project>>change MCU/Connection",Does which codewarrior support MC9S12XEA256? OR Is there a way to add the device?

Labels (1)
0 Kudos
Reply
1 Solution
1,594 Views
TICS_Fiona
NXP Employee
NXP Employee

There is no MC9S12XEA256 in the selection list when creating a new project CodeWarrior, however Processor Expert support this device. 

Since the 9S12XEA128/256 are a special bondouts for access to extra ADC channels in 80QFP, and the MC9S12XEA256 is similar to MC9S12XET256-80QFP. User can first create a new project with wizard for MC9S12XET256, selecting Processor Expert at "Rapid Application Development Options".

After create the project with Processor Expert, add the CPU component for MC9S12XEA128_80 to replace MC9S12XET256.

Hope this will help you.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,595 Views
TICS_Fiona
NXP Employee
NXP Employee

There is no MC9S12XEA256 in the selection list when creating a new project CodeWarrior, however Processor Expert support this device. 

Since the 9S12XEA128/256 are a special bondouts for access to extra ADC channels in 80QFP, and the MC9S12XEA256 is similar to MC9S12XET256-80QFP. User can first create a new project with wizard for MC9S12XET256, selecting Processor Expert at "Rapid Application Development Options".

After create the project with Processor Expert, add the CPU component for MC9S12XEA128_80 to replace MC9S12XET256.

Hope this will help you.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------