MY QUESTIONS ARE HERE:
1. IS KINETIS M0+ SUPPORT EXTERNAL MEMORY BUFFER?
2. WHAT IS THE MAX. SIZE UP TO?
3. DOES ANYONE HAS PRACTICE DCASE / SAMPLE CODES?
Hello Bright,
If you want to use SRAM/SDRAM , i'm sorry to say KEA does not have this kind of
interface, it need flex bus moudle which only exist on K series .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
So Does It Work If I Use I2C / SPI Interface of KEA With RAM Like Cypress's FRAM?http://www.cypress.com/file/41666/download
Alice_Yang <admin@community.freescale.com> 於 2016/9/19 (週一) 3:46 PM 寫道﹕
#yiv3277776569 * #yiv3277776569 a #yiv3277776569 body {font-family:Helvetica, Arial, sans-serif;}#yiv3277776569 #yiv3277776569 h1, #yiv3277776569 h2, #yiv3277776569 h3, #yiv3277776569 h4, #yiv3277776569 h5, #yiv3277776569 h6, #yiv3277776569 p, #yiv3277776569 hr {}#yiv3277776569 .yiv3277776569button td {}
|
NXP Community |
|
Re: IS IT POSSIBLE TO USE SDRAM / SRAM WITH KEA SERIES MCU?
reply from Alice_Yang in CodeWarrior for MCU - View the full discussionHello Bright, If you want to use SRAM/SDRAM , i'm sorry to say KEA does not have this kind ofinterface, it need flex bus moudle which only exist on K series . Hope it helps
Have a great day,
Alice
Hello Wang,
From the datasheet of FRAM, i think in theory it can work use the I2C interface,
while there is no demo .
BR
Alice