Hi.
GB60 is ARCHIVED product which is no longer for new design recommendation.
both classic CW6.3 and eclipse CW10.7 can support GB60. but please note:
- CW6.3 doesn't support 64bit win7 platform but 10.7 does.
- because GB60 is very old product, nearly all the existing demo codes are based on CW6.3 but not CW10.7.
here is the link of CW6.3
CodeWarrior for Microcontrollers-Classic IDE|NXP
here is the link of CW10.7
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
here is demo code of GB60 demo board
GB60 modules demo code is attached.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Jennie and Alice,
The M68DEMO908GB60.zip sample code is in assembly language. I am looking for the sample code in C language.
Appreciate if you could point to the link with the sample code in C language.
Thanks
HI Dang,
unfortunately we don't have the same C demo code M68DEMO908GB60.zip
However I found we have
http://cache.nxp.com/files/microcontrollers/doc/user_guide/HCS08QRUG.pdf
GB60 modules demo code is attached. I suggest you look it though, this will help you better understand HCS08 peripheral usage.
Best Regards.
Jennie
Hello Jennie,
Thank for the info and the sample code. That what is looking for.
Regards,
Minh Dang
Hi.
GB60 is ARCHIVED product which is no longer for new design recommendation.
both classic CW6.3 and eclipse CW10.7 can support GB60. but please note:
- CW6.3 doesn't support 64bit win7 platform but 10.7 does.
- because GB60 is very old product, nearly all the existing demo codes are based on CW6.3 but not CW10.7.
here is the link of CW6.3
CodeWarrior for Microcontrollers-Classic IDE|NXP
here is the link of CW10.7
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
here is demo code of GB60 demo board
GB60 modules demo code is attached.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jennie
The <https://community.nxp.com/servlet/JiveServlet/download/2028-438392-849405-395441/M68DEMO908GB60.zip> M68DEMO908GB60.zip sample code is in assembly language. I am looking for the sample code in C language.
Appreciate if you could point to the link with the sample code in C language.
Thanks
Hello minh,
You can use the lasted version of CWv10.7:
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
it supports this chip.
In CW , create one project with Processor Expert , there will be demo :
when create project select "Processor Expert":
For example the AsynchroSerial demo :
Hope it helps
Alice