Hello,
Hiwave 6.1 crashs when a step-by-step execution is requested inside a function which is launched by an ISR (a 2 ms periodic ISR is used to schedule some tasks).
Debugging these routines is impossible if I can't step into!
thank you for your help!
MCU : MC9S12G240
Operative sistem: Windows 7
These the details of the crash:
Firma problema:
Nome evento problema: APPCRASH
Nome applicazione: hiwave.exe
Versione applicazione: 6.1.44.10221
Timestamp applicazione: 4c6149ce
Nome modulo con errori: msvcrt.dll
Versione modulo con errori: 7.0.7601.17744
Timestamp modulo con errori: 4eeaf722
Codice eccezione: c0000005
Offset eccezione: 0002dc97
Versione SO: 6.1.7601.2.1.0.256.48
ID impostazioni locali: 1040
Informazioni aggiuntive 1: 20cb
Ulteriori informazioni 2: 20cba655bdb47ca2f1c2b0d778505346
Ulteriori informazioni 3: b96f
Ulteriori informazioni 4: b96f01fed0fdf83742e9a6043522ed4d
解決済! 解決策の投稿を見る。
Hello Alessandro Serafini,
from your post your hiwave should be from CW5.1 package, which can support 64bit win7.
I ever have customer met CW crash problem on win7. he solved the problem in this way:
- Right click IDE.exe in the \bin folder.
- Select “Properties”
- Select “Compatibility”
- Select “Change settings for all users”
- Select “Run this program in compatibility mode for”
- Select “Windows 7” from pull down menu
- Select “Disable visual themes” & “Disable desktop composition” &” Disable display scaling on high DPI settings”.
- Do NOT select “Run in 256 colors” & “Run in 640x480 screen resolution”.
- Hit OK.
can you please try it too?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Alessandro Serafini,
from your post your hiwave should be from CW5.1 package, which can support 64bit win7.
I ever have customer met CW crash problem on win7. he solved the problem in this way:
- Right click IDE.exe in the \bin folder.
- Select “Properties”
- Select “Compatibility”
- Select “Change settings for all users”
- Select “Run this program in compatibility mode for”
- Select “Windows 7” from pull down menu
- Select “Disable visual themes” & “Disable desktop composition” &” Disable display scaling on high DPI settings”.
- Do NOT select “Run in 256 colors” & “Run in 640x480 screen resolution”.
- Hit OK.
can you please try it too?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jennie,
first of all thank you for your helop!
I use CW5.1.
following the information on the CW5.1
On your answer on the forum you suggest to select compatibility to Windows Vista. Do you mean Windows 7, right? At the moment seems work OK, I’ll make some checks than I’ll give you the positive answer to the forum.
On my question to the forum I reported the screenshot of the crash (sorry for description in Italian).
Best regards!
Alessandro
Zadi Spa
Alessandro Serafini
HS Engineer
Phone: +39 059 6323111
Fax: +39 059 6323298
E-mail: <mailto:alessandro.serafini@zadi.com> alessandro.serafini@zadi.com
Le informazioni contenute in questa comunicazione e gli eventuali documenti allegati hanno carattere confidenziale, sono tutelate dal segreto professionale e sono ad uso esclusivo del destinatario. Nel caso questa comunicazione Vi sia pervenuta per errore, Vi informiamo che la sua diffusione e riproduzione è contraria alla legge e preghiamo di darci prontamente avviso e di cancellare quanto ricevuto. Grazie.
This e-mail message and any files transmitted with it are subject to attorney-client privilege and contain confidential information intended only for the person(s) to whom it is addressed. If you are not the intended recipient, you are hereby notified that any use or distribution of this e-mail is strictly prohibited: please notify the sender and delete the original message. Thank you
Da: ZhangJennie
Inviato: giovedì 14 gennaio 2016 08:42
A: Alessandro Serafini <alessandro.serafini@zadi.com>
Oggetto: Re: - Hiwave 6.1 crash on Windows 7
<http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1tt/i0C_bbziRNiTpqJMOEDNiQ/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQJ6kyiZ2Cef2qt-2B2uYN1YnWHaJNGi7m0dsLcrT7D0aEsRC9ydi8bGmPSoTrNqropzOzEJWlRcWGPjR3DG2V-2Fd9JgazgrYhAttaPsLKIUR-2FzQ-3D-3D> NXP Community
Hiwave 6.1 crash on Windows 7
reply from ZhangJennie <http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1tt/i0C_bbziRNiTpqJMOEDNiQ/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTuA0ocwt5VQBPvrZ0tSaGYjDWuKJVj0d0rHTz7WLwU2bRpoUFCZp0KGFEP3QCt5Zs-3D> in CodeWarrior for MCU - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/-AA/PDcDAA/t.1tt/i0C_bbziRNiTpqJMOEDNiQ/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bT2TLVfogSPI90FMZxxFFwErQ3ZRR3VzBRVSfxeX-2FUpL05lRBF3C9p9hE1b-2F2zu-2FDY-3D>
hi Alessandro,
yes, I mean windows7.
the solution is the same for vista and windows7 . I will correct it in my original reply right now. thanks.
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jennie,
Your answer is correct. Thank you!
I ‘m sorry but I’m confirmed as right answer my second post.
May you change on the forum and delete the right answer?
Thank you!
Zadi Spa
Alessandro Serafini
HS Engineer
Phone: +39 059 6323111
Fax: +39 059 6323298
E-mail: <mailto:alessandro.serafini@zadi.com> alessandro.serafini@zadi.com
Le informazioni contenute in questa comunicazione e gli eventuali documenti allegati hanno carattere confidenziale, sono tutelate dal segreto professionale e sono ad uso esclusivo del destinatario. Nel caso questa comunicazione Vi sia pervenuta per errore, Vi informiamo che la sua diffusione e riproduzione è contraria alla legge e preghiamo di darci prontamente avviso e di cancellare quanto ricevuto. Grazie.
This e-mail message and any files transmitted with it are subject to attorney-client privilege and contain confidential information intended only for the person(s) to whom it is addressed. If you are not the intended recipient, you are hereby notified that any use or distribution of this e-mail is strictly prohibited: please notify the sender and delete the original message. Thank you
Da: ZhangJennie
Inviato: giovedì 14 gennaio 2016 11:05
A: Alessandro Serafini <alessandro.serafini@zadi.com>
Oggetto: Re: - Hiwave 6.1 crash on Windows 7
<http://jiveon.jivesoftware.com/mpss/c/9AA/PDcDAA/t.1tt/akX6iIY-Tg-ZqL6-m9rqNA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQJ6kyiZ2Cef2qt-2B2uYN1YnWHaJNGi7m0dsLcrT7D0aEsRC9ydi8bGmPSoTrNqropzOzEJWlRcWGPjR3DG2V-2Fd9JgazgrYhAttaPsLKIUR-2FzQ-3D-3D> NXP Community
Hiwave 6.1 crash on Windows 7
reply from ZhangJennie <http://jiveon.jivesoftware.com/mpss/c/9AA/PDcDAA/t.1tt/akX6iIY-Tg-ZqL6-m9rqNA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTuA0ocwt5VQBPvrZ0tSaGYjDWuKJVj0d0rHTz7WLwU2bRpoUFCZp0KGFEP3QCt5Zs-3D> in CodeWarrior for MCU - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/9AA/PDcDAA/t.1tt/akX6iIY-Tg-ZqL6-m9rqNA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ4puxYsxmn-2Fcqs7d5L8-2FfhORg3f8KrT0DUeAE2-2B1R4NiLbs4bQarYKHYLCVYrV-2BXY-3D>
Hi Alessandro Serafini,
It's done.
Thanks!
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jennie,
thank you very much!
Best regards
Zadi Spa
Alessandro Serafini
HS Engineer
Phone: +39 059 6323111
Fax: +39 059 6323298
E-mail: <mailto:alessandro.serafini@zadi.com> alessandro.serafini@zadi.com
Le informazioni contenute in questa comunicazione e gli eventuali documenti allegati hanno carattere confidenziale, sono tutelate dal segreto professionale e sono ad uso esclusivo del destinatario. Nel caso questa comunicazione Vi sia pervenuta per errore, Vi informiamo che la sua diffusione e riproduzione è contraria alla legge e preghiamo di darci prontamente avviso e di cancellare quanto ricevuto. Grazie.
This e-mail message and any files transmitted with it are subject to attorney-client privilege and contain confidential information intended only for the person(s) to whom it is addressed. If you are not the intended recipient, you are hereby notified that any use or distribution of this e-mail is strictly prohibited: please notify the sender and delete the original message. Thank you
Da: ZhangJennie
Inviato: venerdì 15 gennaio 2016 10:53
A: Alessandro Serafini <alessandro.serafini@zadi.com>
Oggetto: Re: - Hiwave 6.1 crash on Windows 7
<http://jiveon.jivesoftware.com/mpss/c/9AA/PDcDAA/t.1tu/_4mb045oQV2xQJTYcMuzfA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQJ6kyiZ2Cef2qt-2B2uYN1YnWHaJNGi7m0dsLcrT7D0aEsRC9ydi8bGmPSoTrNqropzOzEJWlRcWGPjR3DG2V-2Fd9JgazgrYhAttaPsLKIUR-2FzQ-3D-3D> NXP Community
Hiwave 6.1 crash on Windows 7
reply from ZhangJennie <http://jiveon.jivesoftware.com/mpss/c/9AA/PDcDAA/t.1tu/_4mb045oQV2xQJTYcMuzfA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTuA0ocwt5VQBPvrZ0tSaGYjDWuKJVj0d0rHTz7WLwU2bRpoUFCZp0KGFEP3QCt5Zs-3D> in CodeWarrior for MCU - View the full discussion <http://jiveon.jivesoftware.com/mpss/c/9AA/PDcDAA/t.1tu/_4mb045oQV2xQJTYcMuzfA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSHuwY5qUN2hb7bCAnemU0EDWt20WWK8U9bFdcg8XMmEN9vKhOoJh8B6ChaLWZ7ykY-3D>