Hello Community,
Right now, I'm working on a wifi project. I use MQX 4.0.2 and installed Patch for TWR-WIFI-AR4100P. I run some demos in "atheros_wifi" folder and they work well. As I understand, all the original demo projects are linked to the wifi library files and use the functions in those files but if I create my own MQX project in CW it doesn't link to those wifi library. I tried to copy the compiler and assembler input from the demo project to my project but still I get some errors. I tried to copy one of the demos in another location and customized it but that causes the link broken to the wifi library! So my question is how can I create a project and link to the wifi library?
The MQX tools (plugin) doesn't work with any of the demo projects.
I import web_hvac demo by drag and drop “.project” file of the project in CW 10.5 projects window and built it. Do I need to try another import approach? I appreciare you feedback.
Cheers!
解決済! 解決策の投稿を見る。
Hello Jorge,
The way I solved this issue is easy but time consuming. Basically I created a new project using New MQX project Wizard. In the wizard I added rtcs library by right click on source folder and click on "add file". After that I added all AR4100-wifi library files from Qualcomm. The library is huge but after adding all files the project up and running. right now, I am able to debug the code and use MQX tool for task monitoring in my project.
Cheers!
Hello Jorge,
The way I solved this issue is easy but time consuming. Basically I created a new project using New MQX project Wizard. In the wizard I added rtcs library by right click on source folder and click on "add file". After that I added all AR4100-wifi library files from Qualcomm. The library is huge but after adding all files the project up and running. right now, I am able to debug the code and use MQX tool for task monitoring in my project.
Cheers!
Hello:
As far as I know there are no wifi libraries (or you mean the atheros source/header files?). The code for the TWR-WIFI is merged with the default MQX libraries.
So, to use that code you just need to include the required libraries for your new project. If you open the web_hvac demo from the atheros_wifi folder, you can see the linked libraries by going to Project -> Properties -> C/C++ Build -> Settings. In the next 2 example pictures you can see the settings for the TWR-K60D100 project:
1- If using Freescale build tools you would see this:
2- If using GCC build tools:
Hope this is useful!
Regards!
Jorge Gonzalez