Hi,
I would like to know the difference between HCS08 configuration and FLASH configuration.Whether the HCS08 configuration is used for debugging ?Whether FLASH configuration can be used for debugging.
For my project,when I tried to build and compiler ,it gives erros for HCS08 configuration for overlapping of segments.Please find the attachment ,but when I compile with FLASH Configuration for the same .prm file ,it does not give erros and produces a .sx file.Whether there any specific settings apart of changing the configuration
已解决! 转到解答。
Hello Preetu,
This HCS08 configuration is just a basic configuration ,
it need configured by customer refer to customers' demand .
If only select it , then configure nothing, when build , it will show error .
For example , you can create one simple project to have a try ,
in the "HCS08 compiler" selection , the HCS08 configuration have not include all the
header files :
So I recommend you use the FLASH configuration .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Preetu,
From the error , in generally there maybe some definition overlap at the same address ,
please check these address
If you have not checked it out, you can also send your project to me .
Hope it helps
Alice
The chip used is MC9S08GT60 . The configuration for HCS08 is selected from the drop down men which also has FLASH Configuration. I got to know the overlap definition at the same address and when i fixed those erros, it shows a error regardinng allocation of ROM going out of space,
The definition overlap was due to the errors since some variables was defined explicitly defined with address in .c files
So my question is whether the same PRM File cannot be used for both FLASH and HCSO8.
I would like to know the difference between HCS08 configuration and FLASH configuration.Whether the HCS08 configuration is used for debugging ?Whether FLASH configuration can be used for debugging.
Hello Preetu,
From your screenshot i think maybe you use the CW 10.6 , right ?
If yes , when we create one HCS08 project ,the default configuration is Flash configuration,
there is no HSC08 configuration :
So the HCS08 configuration is configured by customer , from check the contents between the two
configuration to the difference :
Regards
Alice
Hello Preetu,
This HCS08 configuration is just a basic configuration ,
it need configured by customer refer to customers' demand .
If only select it , then configure nothing, when build , it will show error .
For example , you can create one simple project to have a try ,
in the "HCS08 compiler" selection , the HCS08 configuration have not include all the
header files :
So I recommend you use the FLASH configuration .
Hope it helps
Have a great day,
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------