CW for MCU, Eclipse 10.4, 56F8367 issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW for MCU, Eclipse 10.4, 56F8367 issue

1,019件の閲覧回数
Ben
Senior Contributor I

I developed a project for the 56F8367. It runs good with the pod attached, by selecting RUN or DEBUG.

However, while programming the internal flash and trying to run it in stand-alone mode, it does not run correctly.

The mail background loop run, but there is no response to events, and it looks that reading RAM parameters is wrong too.

 

I am running another project which has been developed with the same IDE & compiler for the 56F8257, and it run in stand-alone mode perfectly.

Can someone assist? Advice I got to my S/R did not help...

 

TIA

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

779件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Ben,

Do you have a SR number for this problem ?

I've created a project for EVM board on my DSC V8.3 and imported it under MCU V10.2.

this example is running fine.

The application is loaded on board and after a reset it's launched fine.

Now I launch MCU V10.4 and import the project.

The application is working fine too.

After a reset the application is launched.

Attached you will find the project used.

Regards

Pascal