CW for MCU, Eclipse 10.4, 56F8367 issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CW for MCU, Eclipse 10.4, 56F8367 issue

540 次查看
Ben
Senior Contributor I

I developed a project for the 56F8367. It runs good with the pod attached, by selecting RUN or DEBUG.

However, while programming the internal flash and trying to run it in stand-alone mode, it does not run correctly.

The mail background loop run, but there is no response to events, and it looks that reading RAM parameters is wrong too.

 

I am running another project which has been developed with the same IDE & compiler for the 56F8257, and it run in stand-alone mode perfectly.

Can someone assist? Advice I got to my S/R did not help...

 

TIA

标签 (1)
标记 (2)
0 项奖励
1 回复

300 次查看
trytohelp
NXP Employee
NXP Employee

Hi Ben,

Do you have a SR number for this problem ?

I've created a project for EVM board on my DSC V8.3 and imported it under MCU V10.2.

this example is running fine.

The application is loaded on board and after a reset it's launched fine.

Now I launch MCU V10.4 and import the project.

The application is working fine too.

After a reset the application is launched.

Attached you will find the project used.

Regards

Pascal