Hello everybody.
Today I started with CodeWarrior trying to open a collegue´s project in my PC. First of all, my CodeWarrior version is not the same as the one of the project, and I don´t know how much can it affect.
After opening the project folder in the workspace I try to clean it and this error message appears:
mingw32-make: *** No rule to make target `C:\Documents and Settings\Administrador\workspace\Estimulador_mag\Sources\Estimulador.c', needed by `Sources/Estimulador_c.obj'. Stop.
I attach the project's folders.
HI
Are you sure below path/file existing on your computer:
C:\Documents and Settings\Administrador\workspace\Estimulador_mag\Sources\Estimulador.c
Besides, Please check your path settings here in your project properties setting. make sure all settings are correct.
If still have problem, send your project here. I will check it directly.
Best Regards
Jun Zhang
I downloaded your testing code and tried it into my CodeWarrior version. This message of error appeared when cleaning the project...
Which CodeWarrior version do you have installed? Where do you create the workspace folder?
I use CW11.0. I think 11.1 should also work.
Build on my side again. Pass build as well.
Your project doesn't include FLASH_SDM linker file. the related folder has FLASH_LDM file only.
please check the original project owner to provide SDM linker file for building FLASH_SDM configuration.
Jun Zhang