I can't compile "bsp-nto650-freescale-imx53-qsb-sp1-trunk-201209071552.zip" from the Freescale website in the IDE.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I can't compile "bsp-nto650-freescale-imx53-qsb-sp1-trunk-201209071552.zip" from the Freescale website in the IDE.

676 次查看
ballerzhu
Contributor I

Hello,

     I can't compile the BSP of  I.MX53 in the IDE.

It  always presents errors that are "Unable to to find startup: startup-mx53qsb" and

" *** No rule to make target `libinput.a', needed by `D:/QNX-IDE-projectp-freescale-imx53-qsb888-src/src/hardware/devi/mc34708".

I use "bsp-nto650-freescale-imx53-qsb-sp1-trunk-201209071552.zip" from the Freescale website.

Can you help me?

     Thanks very much.

标签 (1)
0 项奖励
回复
1 回复

534 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Baller

this BSP is provided by qnx, suggest to post question on its wiki:

http://community.qnx.com/

I.MX53 QSB Freescale BSPs are based on ltib and located on

Board Support Packages (8)

i.MX53 Quick Start Board|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复