dsp56805 flash.cfg

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

dsp56805 flash.cfg

跳至解决方案
937 次查看
zaur0555
Contributor I

Help me please i need the dsp56805 flash.cfg for program DSP56F805 with Codewarrior USB TAP.

 

0 项奖励
回复
1 解答
852 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you have source code and project, you can use CodeWarrior for DSP56800E ver8.3 tools and generate the file and download via usbtap device.

If you just have S-Record file, you have to use FlashOverJtag.exe tools and Wiggler with PC with 25 pin printer port.

Hope it can help you

BR

XiangJun Rong

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
878 次查看
zaur0555
Contributor I

How can i download CodeWarrior 8.2.3 ?

0 项奖励
回复
920 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to use the file I attached.

Pls try to change the extension name from txt to cfg, because I can not attach the file with cfg as extension name.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复
910 次查看
zaur0555
Contributor I
Hi. I tried but this file doesn't work on 56800E Flash Programmer on CodeWarrior 8.3.
I have .s file and can't programming it to dsp56805 MCU.
0 项奖励
回复
903 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the DSP56F805 was launched in Motorola in 2000 year, it uses DSP56800 core instead of DSP56800E core, so the 56800E Flash Programmer does not support DSP56F805.

You have to use flashoverjtag.exe tools to download code via JTAG with Wiggler(parallel command converter) and PC with 25 pin printer port.

If you use USBTAP device, you have to use CodeWarrior for DSP56800E ver8.3 tools, but the CodeWarrior for DSP56800E ver8.3 tools can work on Win XP, it has issue to run on Win 10 OS.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复
894 次查看
zaur0555
Contributor I

Could you explain how can i flash the  .s file into dsp56f805 via usb tap on code warrior 8.3 please.

0 项奖励
回复
853 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you have source code and project, you can use CodeWarrior for DSP56800E ver8.3 tools and generate the file and download via usbtap device.

If you just have S-Record file, you have to use FlashOverJtag.exe tools and Wiggler with PC with 25 pin printer port.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复
839 次查看
zaur0555
Contributor I

Thank you.

0 项奖励
回复