dsp56805 flash.cfg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dsp56805 flash.cfg

Jump to solution
603 Views
zaur0555
Contributor I

Help me please i need the dsp56805 flash.cfg for program DSP56F805 with Codewarrior USB TAP.

 

0 Kudos
Reply
1 Solution
518 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you have source code and project, you can use CodeWarrior for DSP56800E ver8.3 tools and generate the file and download via usbtap device.

If you just have S-Record file, you have to use FlashOverJtag.exe tools and Wiggler with PC with 25 pin printer port.

Hope it can help you

BR

XiangJun Rong

 

View solution in original post

0 Kudos
Reply
7 Replies
544 Views
zaur0555
Contributor I

How can i download CodeWarrior 8.2.3 ?

0 Kudos
Reply
586 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls try to use the file I attached.

Pls try to change the extension name from txt to cfg, because I can not attach the file with cfg as extension name.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply
576 Views
zaur0555
Contributor I
Hi. I tried but this file doesn't work on 56800E Flash Programmer on CodeWarrior 8.3.
I have .s file and can't programming it to dsp56805 MCU.
0 Kudos
Reply
569 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the DSP56F805 was launched in Motorola in 2000 year, it uses DSP56800 core instead of DSP56800E core, so the 56800E Flash Programmer does not support DSP56F805.

You have to use flashoverjtag.exe tools to download code via JTAG with Wiggler(parallel command converter) and PC with 25 pin printer port.

If you use USBTAP device, you have to use CodeWarrior for DSP56800E ver8.3 tools, but the CodeWarrior for DSP56800E ver8.3 tools can work on Win XP, it has issue to run on Win 10 OS.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply
560 Views
zaur0555
Contributor I

Could you explain how can i flash the  .s file into dsp56f805 via usb tap on code warrior 8.3 please.

0 Kudos
Reply
519 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you have source code and project, you can use CodeWarrior for DSP56800E ver8.3 tools and generate the file and download via usbtap device.

If you just have S-Record file, you have to use FlashOverJtag.exe tools and Wiggler with PC with 25 pin printer port.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply
505 Views
zaur0555
Contributor I

Thank you.

0 Kudos
Reply