cant get mpc8308 in codewarrior config file list

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cant get mpc8308 in codewarrior config file list

ソリューションへジャンプ
2,362件の閲覧回数
startup
Contributor I

codewarrior version used:- CW Power Architecture,Professional Edition,v 8.8 , Build 80229 with XP

Problem:- I am not getting option mpc8308 target processor menu or config file menu instead 8313 is present.

 

Also  when I am running from codewrrior its showing config file error ,jtag not connected so I am suspecting I am not selecting proper target processor.

 

Please tell me whether selecting 8313 is ok instead of 8303(which is not present in the list).

ラベル(1)
0 件の賞賛
返信
1 解決策
841件の閲覧回数
J2MEJediMaster
Specialist I
0 件の賞賛
返信
4 返答(返信)
842件の閲覧回数
J2MEJediMaster
Specialist I

 Check this https://community.freescale.com/message/65680#65680 and see if it helps you.

 

---Tom

0 件の賞賛
返信
841件の閲覧回数
startup
Contributor I

Thanks Tom it helped.

0 件の賞賛
返信
841件の閲覧回数
TekGuy
Contributor I

Hello people.

 

I updated with the patches and now have PowerPC 8308 as a processor type.

But I do not find the MPC8308-RDB as a board option.

I only see 8308 mlTX (rev1), e300_ISS, and Generic.

 

Is the RDB board option available?  Any hints on what to do?

 

Thanks in advance.

0 件の賞賛
返信
841件の閲覧回数
ronco
NXP Employee
NXP Employee

You're right, the 8.8.3 CodeWarrior for Power Architecture does not yet support the MPC8308-RDB, but there is a way you can still work with this board.  Start by creating a CW project for the MPC8308-mITX.  Then change the Target Initialization file in the "EPPC Debugger Settings" panel to '8308erdb_init.cfg' which is included with the BSP for the MPC8308E-RDB (also attached here.)  The BSP can be found at www.freescale.com/powerbsp.   I hope this helps.

 

Regards,

Ron

0 件の賞賛
返信